9065CT9701R03/21

Other Features

Standard Features

Optional Features

  • Repeat trip accuracy: ± 2%

  • Normally closed trip contact

  • Visible trip indication

  • Trip free operation

  • Harmonic immunity

  • Thermal memory

  • Trip test function

  • Three-second trip on phase imbalance ≥ 25% (see Class 9999 Motor Logic Overload Relays Accessories)

  • Auxiliary contacts

  • Electrical remote reset

  • Lug-lug kits for separate mounting

  • DIN rail adapter bracket (00B, 00C, 0, 1)

  • Lug extender kit for retrofit (00B, 00C, 0, 1)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.