9065CT9701R03/21

Table 74

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 74

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

2.23–2.47

2.23–2.47

FB3.33

2.48–2.76

2.48–2.76

FB3.71

2.77–3.04

2.77–3.04

FB4.1

3.05–3.24

3.05–3.24

FB4.5

3.25–3.61

3.25–3.61

FB4.75

3.62–4.19

3.62–4.19

FB5.3

4.20–4.62

4.20–4.62

FB6.1

4.63–5.14

4.63–5.14

FB6.75

5.15–5.39

5.15–5.39

FB7.45

5.40–5.69

5.40–5.69

FB7.8

5.70–5.99

5.70–5.99

FB8.21

6.00–6.29

6.00–6.29

FB8.6

6.30–6.64

6.30–6.64

FB9.0

6.65–6.99

6.65–6.99

FB9.5

7.00–7.39

7.00–7.39

FB10.0

7.40–7.79

7.40–7.79

FB10.6

7.80–7.94

7.80–7.94

FB11.2

7.95–8.49

7.95–8.49

FB12.1

8.50–8.99

8.50–8.99

FB13.1

9.00–9.59

9.00–9.59

FB13.9

9.60–10.1

9.60–10.1

FB14.8

10.2–10.6

10.2–10.6

FB15.6

10.7–11.3

10.7–11.3

FB16.4

11.4–12.0

11.4–12.0

FB17.6

12.0–12.6

FB18.4

12.7–13.8

FB19.4

13.9–14.7

FB21.1

14.8–15.2

FB22.6

15.3–16.2

FB23.6

16.3–18.0

FB24.8

Following Selections for Size 1 Only.

12.0–12.6

FB18.4

12.7–13.8

FB19.4

13.9–14.7

13.9–14.7

FB21.1

14.8–15.2

14.8–15.2

FB22.6

15.3–16.2

15.3–16.2

FB23.6

16.3–17.4

16.3–17.4

FB24.8

17.5–18.5

17.5–18.5

FB26.7

18.6–19.6

18.6–19.6

FB28.3

19.7–20.2

19.7–20.2

FB29.6

20.3–21.5

20.3–21.5

FB30.5

21.6–22.4

21.6–22.4

FB32.6

22.5–23.2

22.5–23.2

FB34.1

23.3–24.3

23.3–24.3

FB35.0

24.4–25.4

24.4–25.4

FB36.6

25.5–26.0

25.5–26.0

FB38.3

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.