9065CT9701R03/21

Table 73

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 73

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

2.42–2.67

2.42–2.67

FB3.33

2.68–3.00

2.68–3.00

FB3.71

3.01–3.36

3.01–3.36

FB4.1

3.37–3.53

3.37–3.53

FB4.5

3.54–3.91

3.54–3.91

FB4.75

3.92–4.41

3.92–4.41

FB5.3

4.42–4.83

4.42–4.83

FB6.1

4.84–5.45

4.84–5.45

FB6.75

5.46–5.89

5.46–5.89

FB7.45

5.90–6.04

5.90–6.04

FB7.8

6.05–6.55

6.05–6.55

FB8.21

6.56–6.72

6.56–6.72

FB8.6

6.73–7.00

6.73–7.00

FB9.0

7.01–7.39

7.01–7.39

FB9.5

7.40–7.54

7.40–7.54

FB10.0

7.55–8.41

7.55–8.41

FB10.6

8.42–8.91

8.42–8.91

FB11.2

8.92–9.16

8.92–9.16

FB12.1

9.17–10.0

9.17–10.0

FB13.1

10.1–10.3

10.1–10.3

FB13.9

10.4–11.4

10.4–11.4

FB14.8

11.5–11.8

11.5–11.8

FB15.6

11.9–12.9

11.9–12.9

FB16.4

13.0–13.4

FB17.6

13.5–14.2

FB18.4

14.3–15.1

FB19.4

15.2–18.0

FB21.1

Following Selections for Size M–1 & M–1P Only.

11.5–11.8

FB15.6

11.9–12.9

FB16.4

13.0–13.4

FB17.6

13.5–14.2

FB18.4

14.3–15.1

FB19.4

15.2–17.1

15.2–17.1

FB21.1

17.2–18.0

17.2–18.0

FB22.6

18.1–18.9

18.1–18.9

FB23.6

19.0–19.7

19.0–19.7

FB24.8

19.8–20.9

19.8–20.9

FB26.7

21.0–21.9

21.0–21.9

FB28.3

22.0–23.1

22.0–23.1

FB29.6

23.2–24.3

23.2–24.3

FB30.5

24.4–25.5

24.4–25.5

FB32.6

25.6–26.0

25.6–26.0

FB34.1

Following Selections for Size M–1P Only.

26.1–26.8

FB35.0

26.9–27.3

FB36.6

27.4–28.7

FB38.3

28.8–30.2

FB40.2

30.3–31.9

FB42.0

32.0–36.0

FB44.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.