9065CT9701R03/21

NEMA Style Dimensional Diagrams

NOTE: Sizes 00B and 00C are not actual NEMA sizes. These designations are used to differentiate the lower FLA of these devices from the NEMA Size 00 Motor Logic solid-state overload relay.

NEMA Size 00B, 00C, 0, and 1 Devices

Size 2 Devices

Size 3 Devices

Size 4 Devices

NEMA Size 5 Type S Device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.