9065CT9701R03/21

Table 145

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 145

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

1.00–1.11

0.91–1.02

B1.30

1.12–1.27

1.03–1.15

B1.45

1.28–1.36

1.16–1.27

B1.67

1.37–1.53

1.28–1.39

B1.88

1.54–1.78

1.40–1.61

B2.10

1.79–2.02

1.62–1.84

B2.40

2.03–2.20

1.85–2.03

B2.65

2.21–2.52

2.04–2.34

B3.00

2.53–2.94

2.35–2.69

B3.30

2.95–3.30

2.70–3.02

B3.70

3.31–3.70

3.03–3.39

B4.15

3.71–4.02

3.40–3.65

B4.85

4.03–4.46

3.66–4.04

B5.50

4.47–4.69

4.05–4.28

B6.25

4.70–5.37

4.29–4.85

B6.90

5.38–5.94

4.86–5.38

B7.70

5.95–6.34

5.39–5.71

B8.20

6.35–7.09

5.72–6.39

B9.10

7.10–8.46

6.40–7.53

B10.2

8.47–9.32

7.54–8.34

B11.5

9.33–10.2

8.35–9.14

B12.8

10.3–10.9

9.15–9.74

B14.0

11.0–12.1

9.75–10.7

B15.5

12.2–13.4

10.8–11.8

B17.5

13.5–14.2

11.9–12.2

B19.5

14.3–16.0

12.3–14.4

B22.0

16.1–18.1

14.5–16.4

B25.0

18.2–20.5

16.5–18.9

B28.0

20.6–23.5

19.0–21.3

B32.0

23.6–27.2

21.4–23.3

B36.0

27.3–30.8

23.4–27.9

B40.0

30.9–35.0

28.0–31.4

B45.0

35.1–37.2

B50.0

37.3–40.0

B56.0

For Type DPSG42 & DPSG43, 40 A starter, select any of the Thermal Units from above.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.