9065CT9701R03/21

Expansion Module

LTMEV40FM Module

The expansion module adds the following functions to the TeSys™ T controller:

  • Voltage measurement between phases up to 690 V nominal

  • Four additional inputs

Inputs

  • Four discrete logic inputs (isolated)

  • Two types of power for the inputs: 24 Vdc and 100 to 240 Vac

  • A 24 Vdc LTMR controller can be assembled with a 240 Vac expansion module and vice versa

The LTMEV must be connected to the LTMR controller by a connecting cable.

Expansion Module

Input Control Voltage

Number of Inputs

Supply to the Electronics

Catalog Number

24 Vdc

4

via the LTMR controller

LTMEV40BD

100–240 Vac

4

LTMEV40FM

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.