9065CT9701R03/21

Isolated Auxiliary Contacts

Overload relay auxiliary contacts are available factory installed or in kit form for field installation on motor logic overload relays. These contacts may be used for isolated alarm contact applications.

Isolated Auxiliary Contacts for Motor Logic Overload Relays

For Use With

Parts Kit Description

Catalog Number

Class & Type

NEMA Size*

8536 SA–SJ

00B through 7

N.O. or N.C. Auxiliary Contact
(Field Convertible)

9999AC04

9065 SF, ST

00B through 7

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.