9065CT9701R03/21

Table 2

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 2

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

0.35–0.38

0.30–0.32

B0.44

0.39–0.43

0.33–0.37

B0.51

0.44–0.48

0.38–0.39

B0.57

0.49–0.56

0.40–0.48

B0.63

0.57–0.63

0.49–0.57

B0.71

0.64–0.71

0.58–0.64

B0.81

0.72–0.78

0.65–0.70

B0.92

0.79–0.88

0.71–0.78

B1.03

0.89–0.99

0.79–0.87

B1.16

1.00–1.15

0.88–0.98

B1.30

1.16–1.23

0.99–1.13

B1.45

1.24–1.43

1.14–1.25

B1.67

1.44–1.51

1.26–1.40

B1.88

1.52–1.75

1.41–1.58

B2.10

1.76–1.93

1.59–1.79

B2.40

1.94–2.25

1.80–1.91

B2.65

2.26–2.47

1.92–2.20

B3.00

2.48–2.81

2.21–2.55

B3.30

2.82–3.20

2.56–2.87

B3.70

3.21–3.63

2.88–3.24

B4.15

3.64–4.19

3.25–3.48

B4.85

4.20–4.53

3.49–3.85

B5.50

4.54–4.89

3.86–4.10

B6.25

4.90–5.68

4.11–4.79

B6.90

5.69–6.27

4.80–5.31

B7.70

6.28–6.85

5.32–5.65

B8.20

6.86–7.73

5.66–6.35

B9.10

7.74–8.50

6.36–7.31

B10.2

8.51–9.29

7.32–8.34

B11.5

9.30–10.4

8.35–8.84

B12.8

10.5–11.3

8.85–9.47

B14.0

11.4–12.3

9.48–10.4

B15.5

12.4–13.9

10.5–11.5

B17.5

14.0–15.0

11.6–12.0

B19.5

15.1–18.0

B22.0

Following Selections
for Size M-1 & M-1P Only.

11.6–12.4

B19.5

15.1–17.4

12.5–14.0

B22.0

17.5–19.2

14.1–15.8

B25.0

19.3–22.0

15.9–17.8

B28.0

22.1–24.6

17.9–19.7

B32.0

24.7–26.0

19.8–22.4

B36.0

22.5–25.1

B40.0

25.1–26.0

B45.0

Following Selections
for Size M-1P Only.

24.7–29.1

B36.0

29.2–31.7

B40.0

31.8–36.0

B45.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.