9065CT9701R03/21

Table 148

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 148

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

4.14–4.45

3.70–4.09

B5.50

4.46–4.88

4.10–4.35

B6.25

4.89–5.44

4.36–5.07

B6.90

5.45–6.08

5.08–5.79

B7.70

6.09–6.42

5.80–6.27

B8.20

6.43–7.28

6.28–7.16

B9.10

7.29–8.42

7.17–8.58

B10.2

8.43–9.64

8.59–9.55

B11.5

9.65–10.4

9.56–10.2

B12.8

10.5–11.2

10.3–10.9

B14.0

11.3–12.3

11.0–11.9

B15.5

12.4–13.7

12.0–13.1

B17.5

13.8–14.8

13.2–14.0

B19.5

14.9–16.5

14.1–14.8

B22.0

16.6–18.7

14.9–17.0

B25.0

18.8–21.4

17.1–19.6

B28.0

21.5–24.3

19.7–22.1

B32.0

24.4–28.0

22.2–26.0

B36.0

28.1–33.3

26.1–29.4

B40.0

33.4–37.6

29.5–34.0

B45.0

37.7–41.1

34.1–36.4

B50.0

41.2–44.1

36.5–39.2

B56.0

44.2–47.8

39.3–42.4

B62.0

47.9–50.0

42.5–49.3

B70.0

49.4–50.0

B79.0

For Type DPSO52 & DPSO53, 50 A starter, select any of the Thermal Units from above.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.