9065CT9701R03/21

Table 3

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 3

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

0.29–0.31

0.28–0.29

B0.44

0.32–0.36

0.30–0.33

B0.51

0.37–0.39

0.34–0.36

B0.57

0.40–0.47

0.37–0.44

B0.63

0.48–0.56

0.45–0.52

B0.71

0.57–0.63

0.53–0.59

B0.81

0.64–0.69

0.60–0.64

B0.92

0.70–0.77

0.65–0.71

B1.03

0.78–0.86

0.72–0.80

B1.16

0.87–0.97

0.81–0.90

B1.30

0.98–1.12

0.91–1.03

B1.45

1.13–1.24

1.04–1.14

B1.67

1.25–1.39

1.15–1.27

B1.88

1.40–1.57

1.28–1.44

B2.10

1.58–1.78

1.45–1.63

B2.40

1.79–1.96

1.64–1.79

B2.65

1.97–2.20

1.80–2.01

B3.00

2.21–2.41

2.02–2.19

B3.30

2.42–2.75

2.20–2.52

B3.70

2.76–3.25

2.53–2.95

B4.15

3.26–3.50

2.96–3.17

B4.85

3.51–3.87

3.18–3.50

B5.50

3.88–4.13

3.51–3.73

B6.25

4.14–4.69

3.74–4.22

B6.90

4.70–5.20

4.23–4.68

B7.70

5.21–5.53

4.69–4.98

B8.20

5.54–6.23

4.99–5.59

B9.10

6.24–7.18

5.60–6.43

B10.2

7.19–8.20

6.44–7.41

B11.5

8.21–8.98

7.42–8.02

B12.8

8.99–9.63

8.03–8.59

B14.0

9.64–10.6

8.60–9.52

B15.5

10.7–11.8

9.53–10.5

B17.5

11.9–12.7

10.6–11.2

B19.5

12.8–14.3

11.3–12.0

B22.0

14.4–16.1

B25.0

16.2–18.0

B28.0

Following Selections
for Size M-1 & M-1P Only.

11.3–12.7

B22.0

12.8–14.3

B25.0

16.2–18.3

14.4–16.1

B28.0

18.4–20.2

16.2–17.8

B32.0

20.3–23.0

17.9–20.1

B36.0

23.1–26.0

20.2–22.6

B40.0

22.7–25.5

B45.0

25.6–26.0

B50.0

Following Selections
for Size M-1P Only

25.9–29.0

B45.0

29.1–30.8

B50.0

30.9–32.7

B56.0

32.8–36.0

B62.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.