9065CT9701R03/21

Special Features for Melting Alloy Overload Relays

Special Features for Melting Alloy Overload Relays

Description

Form

Substitute 1-N.O. isolated alarm contact and 1-N.C. contact per relay. (Type S starters only)*

Y342

Substitute 2-N.C. contacts for standard N.C. contact per relay. (Type S starters only)*

Y344

Modify Type SDO12 relays to accept Type FB quick-trip or SB slow-trip thermal units. (Rejects Type CC standard trip units)*

Y81

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.