9065CT9701R03/21

Table 58

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 58

Motor FLC (A)

Thermal Unit Number

1 or 2.T.U.

3 T.U.

3.37–3.82

3.28–3.51

B4.85

3.83–4.33

3.52–3.89

B5.50

4.34–4.79

3.90–4.14

B6.25

4.80–5.33

4.15–4.73

B6.90

5.34–5.79

4.74–5.22

B7.70

5.80–6.27

5.23–5.53

B8.20

6.28–7.03

5.54–6.21

B9.10

7.04–7.88

6.22–7.17

B10.2

7.89–8.73

7.18–8.19

B11.5

8.74–9.55

8.20–8.90

B12.8

9.56–10.6

8.91–9.57

B14.0

10.7–11.8

9.58–10.6

B15.5

11.9–13.1

10.7–11.8

B17.5

13.2–14.9

11.9–12.7

B19.5

15.0–16.9

12.8–14.4

B22.0

17.0–18.8

14.5–16.1

B25.0

18.9–21.5

16.2–18.2

B28.0

21.6–24.1

18.3–20.2

B32.0

24.2–26.8

20.3–22.8

B36.0

26.9–29.9

22.9–25.6

B40.0

30.0–35.5

25.7–28.8

B45.0

35.6–36.5

28.9–30.6

B50.0

36.6–39.6

30.7–32.4

B56.0

39.7–41.5

32.5–34.6

B62.0

41.6–45.0

34.7–38.6

B70.0

38.7–45.0

B79.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.