9065CT9701R03/21

HMI Modules

The following Human Machine Interface (HMI) modules can be used with the motor management system.

  • The LTMCU operator control unit: Control and monitoring of a 1 to 1 LTMR controller.

  • The LTMCUF operator control unit (LTMCU with Fast Device Replacement (FDR) on HMI):

    • Backup and store the configuration and custom logic of the LTMR controller.

    • Facilitate the operator task when replacing a drawer in an environment of high continuity of service without using a computer.

LTMCU Module

The LTMCU Compact Display provides the following functions:

  • Configure the parameters

  • Display information

  • Monitor the alarms and detected faults

  • Local control of the motor via the local control interface (keys can be customized)

  • Three different languages can be loaded into the LTMCU controller at the same time: English, French, Spanish are the defaults.

A language download utility (LangTool), together with all the other languages, are available on the website www.schneider-electric.com.

This tool allows the languages present in the LTMCU control unit to be adapted.

The LTMCU HMI control unit has an additional front panel RJ45 port, protected by a flexible cover.

LTMCUF (LTMCU with FRD on HMI) Module

The LTMCUF Compact Display enables:

  • LTMR monitoring and settings

  • LTMR configuration backup and restoration

  • Copy and paste of configuration at commissioning

Two applications have been predefined for the TeSys T controller. Depending on the application loaded, the HMI terminal makes it possible to:

  • Configure and monitor a motor starter (LTM_1T1_V1.dop)

  • Monitor and modify certain parameters up to 8 motor starters (LTM_1T8_X_V1.dop)

HMI Modules

Description

Supply Voltage

Catalog Number

LTMCU Operator Control unit

via the LTMR controller

LTMCU

LTMCUF with FDR Operator Control unit

via the LTMR controller

LTMCUF
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.