9065CT9701R03/21

Motor Control Modes

Ten predefined motor control modes are incorporated in the controller. Each listed mode is available as two-wire or three-wire control.

  • Overload mode: Monitoring of motors whose control is not managed by the controller

  • Independent mode: Starting of full voltage non-reversing motors

  • Reverser mode: Starting of full voltage reversing motors

  • Two-step mode: Two-step starting of motors (star-delta, by autotransformer and by resistor)

  • Two-speed mode: Two-speed starting of motors (Dahlander, pole changer)

A custom mode is available which allows you to create a specific motor control mode that is not predefined in the controller.

Custom Logic has the basic functions of a small programmable logic controller (PLC). Programming can be done in Structured Text mode or in Block Diagrams through SoMove™ software. To ensure consistency, the same software used to commission the TeSys™ T controller is used for Custom Logic programming.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.