9065CT9701R03/21

Motor Logic™ Solid-State Overload Relays (SSOLRS)

Motor Logic™ Solid-State Overload Relays

Motor Logic solid-state overload relays (SSOLRs) feature:

  • 3 to 1 adjustment for trip current

  • Phase loss and unbalance protection

  • Direct replacement for Type S melting alloy

  • Ambient insensitive and self–powered

  • Switch selectable trip class

  • Class II ground fault detection

  • Electrical remote reset is also available.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.