9065CT9701R03/21

Table 112

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 112

Motor FLC (A)

Thermal Unit Number

44.0–46.8

CC64.3

46.9–50.6

CC68.5

50.7–54.5

CC74.6

54.6–58.4

CC81.5

58.5–62.9

CC87.7

63.0–67.7

CC94.0

67.8–72.9

CC103.0

73.0–78.1

CC112.0

78.2–83.9

CC121.0

84.0–91.1

CC132.0

91.2–97.5

CC143.0

97.6–104

CC156.0

105–113

CC167.0

114–133

CC180.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.