9065CT9701R03/21

Table 81

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 81

Motor FLC (A)

Thermal Unit Number

52.2–55.6

FB50.5

55.7–58.8

FB52.5

58.9–62.5

FB55.5

62.6–66.0

FB58.0

66.1–70.1

FB60.0

70.2–78.6

FB63.5

78.7–92.0

FB69.0

92.1–102

FB77.0

103–114

FB84.0

115–123

FB92.0

124–133

FB105.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.