9065CT9701R03/21

Table 53

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 53

Motor FLC (A)

Thermal Unit Number

1.T.U.

3 T.U.

0.31–0.33

0.29–0.31

B0.44

0.34–0.36

0.32–0.36

B0.51

0.37–0.40

0.37–0.38

B0.57

0.41–0.48

0.39–0.46

B0.63

0.49–0.57

0.47–0.55

B0.71

0.58–0.64

0.56–0.61

B0.81

0.65–0.70

0.62–0.66

B0.92

0.71–0.77

0.67–0.75

B1.03

0.78–0.85

0.76–0.83

B1.16

0.86–0.99

0.84–0.93

B1.30

1.00–1.10

0.94–1.06

B1.45

1.11–1.28

1.07–1.18

B1.67

1.29–1.41

1.19–1.31

B1.88

1.42–1.58

1.32–1.47

B2.10

1.59–1.80

1.48–1.67

B2.40

1.81–2.03

1.68–1.83

B2.65

2.04–2.25

1.84–2.04

B3.00

2.26–2.51

2.05–2.38

B3.30

2.52–2.83

2.39–2.60

B3.70

2.84–3.29

2.61–3.13

B4.15

3.30–3.75

3.14–3.59

B4.85

3.76–4.22

3.60–3.94

B5.50

4.23–4.65

3.95–4.19

B6.25

4.66–5.16

4.20–4.72

B6.90

5.17–5.53

4.73–5.21

B7.70

5.54–6.09

5.22–5.51

B8.20

6.10–6.80

5.52–6.17

B9.10

6.81–7.60

6.18–7.00

B10.2

7.61–8.35

B11.5

8.36–9.00

B12.8

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.