9065CT9701R03/21

Table 78

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 78

Motor FLC (A)

Thermal Unit Number

1 T.U.

2 or 3 T.U.

2.26–2.51

2.26–2.51

FB3.33

2.52–2.82

2.52–2.82

FB3.71

2.83–3.09

2.83–3.09

FB4.1

3.10–3.30

3.10–3.30

FB4.5

3.31–3.69

3.31–3.69

FB4.75

3.70–4.27

3.70–4.27

FB5.3

4.28–4.72

4.28–4.72

FB6.1

4.73–5.25

4.73–5.25

FB6.75

5.26–5.53

5.26–5.53

FB7.45

5.54–5.81

5.54–5.81

FB7.8

5.82–6.14

5.82–6.14

FB8.21

6.15–6.44

6.15–6.44

FB8.6

6.45–6.81

6.45–6.81

FB9.0

6.82–7.19

6.82–7.19

FB9.5

7.20–7.59

7.20–7.59

FB10.0

7.60–7.99

7.60–7.99

FB10.6

8.00–8.17

8.00–8.17

FB11.2

8.18–8.74

8.18–8.74

FB12.1

8.75–9.31

8.75–9.31

FB13.1

9.32–9.94

9.32–9.94

FB13.9

9.95–10.5

9.95–10.5

FB14.8

10.6–11.1

10.6–11.1

FB15.6

11.2–11.9

11.2–12.0

FB16.4

12.0–12.4

FB17.6

12.5–13.1

FB18.4

13.2–14.3

FB19.4

14.4–15.3

FB21.1

15.4–15.9

FB22.6

16.0–18.0

FB23.6

Following Selections for Size 1 Only.

12.0–12.4

FB17.6

12.5–13.1

FB18.4

13.2–14.3

FB19.4

14.4–15.3

14.4–15.3

FB21.1

15.4–15.9

15.4–15.9

FB22.6

16.0–16.9

16.0–16.9

FB23.6

17.0–18.3

17.0–18.3

FB24.8

18.4–19.5

18.4–19.5

FB26.7

19.6–20.5

19.6–20.5

FB28.3

20.6–21.1

20.6–21.1

FB29.6

21.2–22.6

21.2–22.6

FB30.5

22.7–23.7

22.7–23.7

FB32.6

23.8–24.3

23.8–24.3

FB35.0

24.4–26.0

24.4–26.0

FB35.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.