9065CT9701R03/21

Table 72

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 72

Motor FLC (A)

Thermal Unit Number

1 T.U.

3 T.U.

2.38–2.62

2.38–2.62

FB3.33

2.63–2.94

2.63–2.94

FB3.71

2.95–3.31

2.95–3.31

FB4.1

3.32–3.43

3.32–3.43

FB4.5

3.44–3.81

3.44–3.81

FB4.75

3.82–4.32

3.82–4.32

FB5.3

4.33–4.75

4.33–4.75

FB6.1

4.76–5.38

4.76–5.38

FB6.75

5.39–5.75

5.39–5.75

FB7.45

5.76–5.97

5.76–5.97

FB7.8

5.98–6.30

5.98–6.30

FB8.21

6.31–6.55

6.31–6.55

FB8.6

6.56–6.89

6.56–6.89

FB9.0

6.90–7.14

6.90–7.14

FB9.5

7.15–7.36

7.15–7.36

FB10.0

7.37–8.30

7.37–8.30

FB10.6

8.31–8.59

8.31–8.59

FB11.2

8.60–9.01

8.60–9.01

FB12.1

9.02–9.68

9.02–9.68

FB13.1

9.69–9.99

9.69–9.99

FB13.9

10.0–10.9

10.0–10.9

FB14.8

11.0–11.3

11.0–11.3

FB15.6

11.4–12.4

11.4–12.0

FB16.4

12.5–12.9

FB17.6

13.0–14.0

FB18.4

14.1–14.5

FB19.4

14.6–15.7

FB21.1

15.8–16.6

FB22.6

16.7–18.0

FB23.6

Following Selections for Size M–1 & M–1P Only.

11.4–12.4

FB16.4

12.5–12.9

FB17.6

13.0–14.0

FB18.4

14.1–14.5

FB19.4

14.6–15.7

FB21.1

15.8–16.6

FB22.6

16.7–17.6

16.7–17.6

FB23.6

17.7–18.3

17.7–18.3

FB24.8

18.4–19.4

18.4–19.4

FB26.7

19.5–20.5

19.5–20.5

FB28.3

20.6–21.7

20.6–21.7

FB29.6

21.8–22.8

21.8–22.8

FB30.5

22.9–24.3

22.9–24.3

FB32.5

24.4–24.7

24.4–24.7

FB34.1

24.8–25.4

24.8–25.4

FB35.0

25.5–26.0

25.5–26.0

FB36.6

Following Selections for Size M–1P Only.

26.1–27.7

FB38.3

27.8–28.9

FB40.2

29.0–30.6

FB42.0

30.7–32.5

FB44.0

32.6–36.0

FB46.0

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.