9065CT9701R03/21

Communication Protocols

TeSys™ T Motor Management System is a flexible motor management system that supports six major communication protocols:

  • Modbus™

  • CANopen

  • DeviceNet™

  • Profibus

  • Ethernet/IP

  • Modbus/TCP

These communication protocols allow the TeSys T controller to integrate seamlessly into your automation systems.

Ethernet/IP and Modbus/TCP provide Fast/Fault Device Replacement (FDR) to enable quick replacement of products and minimize maintenance time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.