9065CT9701R03/21

Separate Mounting—Melting Alloy Overload Relays

Separate Mounting—Melting Alloy—600 V Maximum, AC or DC*

NEMA Size

Maximum
Full Load
Current (A)

Open Type
for Separate Panel Mounting

Left and Right Hand Types

Open Type Relay and Bracket Kit
for Terminal Block Channel Mounting

Type

NOTE: 3-pole construction (One Common N.C. Contact on Type S Only)—3 Thermal Units Required

00–1

25

9065SEO5

9065SM2

2

45

9065SEO8

9065SM2

3

86

9065SEO12

4

133

9065SEO15

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.