9065CT9701R03/21

Table 5

For additional information and instructions for thermal units, see the previous sections Introduction through Mounting the Thermal Units in this chapter.

Thermal Unit — Table 5

Current Transformer Ratio

Thermal Unit Number

25/5

50/5

75/5

100/5

150/5

200/5

250/5

300/5

400/5

500/5

Motor FLC

10.6–11.7

21.1–23.6

31.7–35.4

42.3–47.2

63.4–70.9

84.5–94.6

106.–117.

127.–141.

169.–188.

211.–236.

B3.00

11.8–13.2

3.7–26.5

35.5–39.8

47.3–53.1

71.0–79.7

94.7–105.

118.–132.

142.–159.

189.–212.

237.–265.

B3.30

13.3–14.8

26.6–29.6

39.9–44.5

53.2–59.4

79.8–89.1

106.–118.

133.–148.

160.–177.

213.–237.

266.–296.

B3.70

14.9–17.2

29.7–34.5

44.6–51.8

59.5–69.2

89.2–103.

119.–138.

149.–172.

178.–207.

238.–276.

297.–345.

B4.15

17.3–19.6

34.6–39.2

51.9–58.9

69.3–78.6

104.–117.

139.–156.

173.–196.

208.–235.

277.–314.

346.–360.

B4.85

19.7–22.3

39.3–44.6

59.0–67.0

78.7–89.3

118.–133.

157.–178.

197.–223.

236.–267.

315.–357.

B5.50

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.