Flow Direction - Electric

The Flow Direction Show Flow Direction button tool provides editors the ability to visualize which direction the network is being fed from the source. This proves useful when trying to determine which areas of the network can be isolated with the smallest impact on customers. For example, with electric networks, you can find where power is being fed and determine which switches can be operated to stop the flow of electricity.

You can control the size, transparency, and color of the flow direction graphics using the Trace options dock pane. The flow direction tool works on facility network data supported by ArcFM Editor XI for electric distribution networks.

To perform a trace with flow direction, follow these steps:

  1. Use the Find Subnetwork tool to locate the area you want to run the trace on.

  2. Click the Show Flow Direction button to start the trace. It may take a moment for the flow direction animation to start.

    Find Subnetwork Tool with Show Flow Direction button highlighted

    Once the animation starts, the display should look something similar to this:

    Show Flow Direction Tool showing the flow of electricity

  3. To turn off the animations, you can click the Show Flow Direction button again or, close out the Find Subnetwork dialog. The Show Flow Direction button appears as a toggle. When the background is white, the tool is turned off. When the background is grey Show Flow Direction button, the tool is turned on.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.