DOCA0189EN–05

Motor ON and Alarm LEDs

LED

LED status

Indication

Motor ON

Green steady

The motor is supplied:

  • On LR9G115 or LR9G225 relays: the current measured is higher than 25 A

  • On LR9G500 or LR9G630 relays: the current measured is higher than 50 A

Green blinking

An overload relay internal malfunction is detected, see Troubleshooting

OFF

The motor is not supplied:

  • On LR9G115 or LR9G225 relays: the current measured is lower than 25 A

  • On LR9G500 or LR9G630 relays: the current measured is lower than 50 A

Alarm

Orange steady

Overload alarm: 90% of the motor thermal capacity is reached

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.