DOCA0189EN–05

Overload Reset Mode Setting and Phase Imbalance Activation

The same rotary switch is used:

  • to enable or disable the automatic reset of the thermal overload protection.

  • to enable or disable the phase imbalance protection.

The thermal overload protection automatic reset is disabled and the phase imbalance protection is enabled.

The thermal overload protection automatic reset is disabled and the phase imbalance protection is disabled.

The thermal overload protection automatic reset is enabled and the phase imbalance protection is enabled.

The thermal overload protection automatic reset is enabled and the phase imbalance protection is disabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.