DOCA0189EN–05

Installation Procedure

Perform the following procedure to install a TeSys Giga contactor on the retrofit base.
  1. Remove the four mounting screws from the fixing holes of the TeSys F contactor.
  2. Remove the TeSys F contactor.
  3. Place the retrofit base on the fixing holes of the TeSys F contactor. Use the holes on the retrofit base corresponding to the TeSys F contactor to replace, as indicated on TeSys Giga Contactor Mounting on Retrofit Base.
  4. Insert and tighten the four mounting screws with PZ2 screwdriver at the right torque.

    NOTE: Use the screws of the TeSys F contactor to install the retrofit base.

  5. Insert and tighten the two short screws (A) half way diagonally on the retrofit base.
  6. Place the TeSys F contactor on the short screws head.
  7. Insert and tighten the long screws (B) with PZ2 screwdriver at the right torque.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.