DOCA0189EN–05

Overview

Based on contact wear or as needed, the switching modules can be replaced. The switching modules must be replaced when the contact wear diagnosis function has detected that the contacts are worn. When the contacts are worn, all switching modules must be replaced together.

The switching modules are compatible with advanced and standard contactors.

The table below provides the commercial references of the switching modules:

Contactor

Set of 3 switching modules for 3P contactor

Set of 4 switching modules for 4P contactors

LC1G115–225

LA9G3QA

LA9G4QA

LC1G265–330

LA9G3RA

LA9G4RA

LC1G400–500

LA9G3SA

LA9G4SA

LC1G630–800

LA9G3TA

LA9G4TA

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.