DOCA0189EN–05

Power Connection with Star Bar Connection Kit

Overview

Star bar connection kit is a single star coupling bar to couple the motor stator windings. It is a spare part for the Star-Delta connection kits.

The table below provides the list of the star bar connection kits:

Contactors

Star bar connection kit

LC1G115-225

LA9GQW601

LC1G265-500

LA9GSW601

LC1G630-800

LA9GTW601

Dimensions

Commercial reference

W

H

X

LA9GQW601

103.7 mm (4.1 in.)

53.25 mm (2.1 in.)

35 mm (1.4 in.)

LA9GSW601

138 mm (5.4 in.)

66.7 mm (2.6 in.)

45mm (1.7 in.)

LA9GTW601

208 mm (8.1 in.)

89 mm (3.5 in.)

70 mm (2.7 in.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.