DOCA0189EN–05

Connection with Box Connectors

Box connectors can be used to connect contactors and overload relays fitted with the following terminal extensions:

  • straight terminal extensions

  • spreaders

  • terminal adapters for box connectors.

The table below provides the list of the box connectors used with the contactors and overload relays:

Contactor

Overload relay

Terminal extension

Box connector

LC1G115-225

LR9G115-225

Straight terminal extensions LA9G●601

AL250●●●

DZ2FG●●●

Spreaders LA9G●611

AL250●●●

DZ2FG●●●

DZ2FH●●●

Terminal adapters for box connectors LA9G●711

AL400●●●

DZ2FH●●●

DZ2FJ●●●

LC1G265-500

LR9G500

Spreaders LA9G●612

AL400●●●

AL600LS52K●

DZ2FJ●●●

DZ2FK●●●

Terminal adapters for box connectors LA9G●712

AL400●●●

AL600LS52K●

DZ2FJ●●●

DZ2FK●●●

LC1G630-800

LR9G630

Terminal adapters for box connectors LA9G●714

AL600●●●

DZ2FK●●●

DZ2FL●●●

Type S

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.