DOCA0189EN–05

Installation of Phase Separator on Overload Relays

  1. See the direction shown on the phase separator according to the contactor rating corresponding to the rating of the overlad relay to insert it on the overload relay power terminals.
  2. Insert the phase separator in the right direction on the power terminals of the overload relay.
  3. Push the phase separator inwards to lock it automatically with a click.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?