DOCA0189EN–05

Trip Class Setting and Ground Fault Activation

The same rotary switch is used:

  • to set the trip class of the thermal overload protection.

  • to enable or disable the ground fault protection.

The ground fault protection is enabled and the thermal overload trip class is set to 10E.

The ground fault protection is disabled and the thermal overload trip class is set to 10E.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?