DOCA0189EN–05

Wiring Characteristics

Cable type

Stripping length

Number of conductors

Section

Solid cable without cable end

12 mm (0.47 in.)

1 conductor

0.75–2.5 mm² (18–14 AWG)

2 conductors

Flexible cable with suitable cable end

10 mm (0.40 in.)

1 conductor

0.75–2.5 mm² (18–14 AWG)

2 conductors

Flexible cable with suitable sleeve

10 mm (0.40 in.)

1 conductor

2 conductors

0.75–2.5 mm² (18–14 AWG)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.