DOCA0189EN–05

Installation of Phase Separator with Coupling Bars

  1. See the direction shown on the phase separator to cut it according to the contactor rating.
  2. Cut the extra part of the phase separator.
  3. Insert the phase separator in the right direction on the power terminals of the contactor.
  4. Push the phase separator inwards to lock it automatically with a click.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?