DOCA0189EN–05

Installation of the Box Connectors

Box connectors can be used to connect contactors and overload relays fitted with the following terminal extensions:

  • straight terminal extensions

  • spreaders

  • terminal adapters for box connectors.

  1. Place the box connector on the terminal extension.

  2. Insert the screw and washer through the box connector and hole at the top of the terminal extension.

  3. Tighten the screws at the right torque.

  4. Place the cable of the power circuit in the box connector.

  5. Tighten the box connector screws at the right torque.

For more information on box connector installation and connection, refer to the instruction bulletin supplied with the box connectors.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.