DOCA0189EN–05

Installation of Phase Separator on Contactors

  1. See the direction shown on the phase separator according to the contactor rating to insert it on contactor power terminals.
  2. Insert the phase separator in the right direction on the power terminals of the contactor.
  3. Push the phase separator inwards to lock it automatically with a click.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.