DOCA0189EN–05

Removal of Contactor without Cable Memory

Before replacing the switching modules on a contactor without cable memory:
  • Remove the mechanical interlock and coupling bars, if present.

  • Remove all auxiliary contact modules.

  • Disconnect top and bottom power connections.

Perform the following procedure to remove the contactor without cable memory:

  1. Unscrew the control terminal blocks.
  2. Remove the control terminal blocks.
  3. Disconnect the top and bottom power connections.
  4. Free the contactor from the power conductors.
  5. Unscrew with an Allen key the 4 screws fixing the contactor block in the contactor housing.
  6. Remove the contactor block from the contactor housing.

Contactor

Tool

Screws

LC1G115-225

Allen key

M8

LC1G265-500

Inner hexagon

M10

LC1G630-800

Inner hexagon

M12

Contactor

Tool

Length of Allen Key (L)

Screws

LC1G115-225

Allen key

≥ 95 mm (≥ 3.74 in.)

M4

LC1G265-500

Allen key

≥ 115 mm (≥ 4.52 in.)

M4

LC1G630-800

Allen key

≥ 115 mm (≥ 4.52 in.)

M6

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.