DOCA0189EN–05

Installation of Phase Separators

  1. Place the phase separator on the power terminals of the contactor.

  2. Push the phase separator inwards to lock it automatically with a click.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.