DOCA0189EN–05

Installation of Remote Wear Diagnostic Module

  1. Press the button of the cap on top of advanced contactor.
  2. Pull the cap on top of advanced contactor.
  3. Place the remote wear diagnostic module on the contactor and push it inwards to lock it automatically with a click.
  4. Connect the cable to lock it automatically with a click.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.