DOCA0189EN–05

Without Remote Wear Diagnosis Module

To reset the wear diagnosis indication after replacement of the switching modules on contactors without remote wear diagnosis module:
  1. Open the cover of the Reset switch

  2. Change the position of the Reset switch on the contactor (from A to B or from B to A).

After reset and after power on A1-A2, the contactor is in reset sequence for 10 s: the diagnosis LED is blinking, and the contactor remains open. It closes after the 10 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.