DOCA0189EN–05

Flexible Terminal Extensions

Flexible connecting bars can be used to connect TeSys Giga advanced or standard contactors with moulded case circuit breakers mounted in the same plane and orientation.

The table below provides the list of flexible terminal extensions used to connect advanced or standard contactors with moulded case circuit breakers:

Contactor

Moulded case circuit breaker

Number of poles

Flexible terminal extensions

LC1G115-225

TeSys Power – Giga Motor Protection Frame 5

3P

LA9G3111

ComPacT NSX100-250

PowerPacT H- / J-Frame

ComPacT NSX100-250

4P

LA9G4111

LC1G265-500

TeSys Power – Giga Motor Protection Frame 6

3P

LA9G3112

ComPacT NSX400-630

PowerPacT L-Frame

ComPacT NSX400-630

4P

LA9G4112

LC1G630-800

ComPacT NS630b-1600

3P

LA9G3113

PowerPacT P-Frame

ComPacT NS630b-1600

4P

LA9G4113

NOTE: To ease the mounting, drilling stencils JYT1902701 can be downloaded from the www.se.com website.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.