DOCA0189EN–05

Ir/FLA Setting

The Ir/FLA setting corresponds to the rated current of the motor or full load amp and can be adjusted with a 56-position rotary switch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.