DOCA0189EN–05

Range

The table below describes the range of the TeSys Giga electronic overload relays :

Commercial reference

Ir/FLA setting range

Direct mounting on contactor

LR9G115

28–115 A

LC1G115–225

LR9G225

57–225 A

LC1G115–225

LR9G500

125–500 A

LC1G265–500

LR9G630

160–630 A

LC1G630–800

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.