DOCA0189EN–05

TeSys Giga Contactor Assembly with TeSys Giga Overload Relay Separately Mounted

Overview

The mounting base is used for separately mounting of overload relay beneath contactor to align the main power pole connections of the contactor and the overload relay, to allow connection between the contactor and the overload relay with straight bars.

Description

Mounting base reference

Mounting base for alignment of LR9G115-225 with LC1G115-225

LA9G3650

Mounting base for alignment of LR9G500 with LC1G265-330

LA9G3651

Mounting base for alignment of LR9G500 with LC1G400-500

LA9G3652

Mounting base for alignment of LR9G630 with LC1G630-800

LA9G3653

Installation Procedure

Perform the following procedure to install the mounting base on the overload relay.

  1. Push outwards the phase separator adaptor from the overload relay.

  2. Remove the phase separator adaptor and keep aside for further use

  3. Place the mounting base on the top hooks at the back of the overload relay.

  4. Push it inwards to lock the mounting base automatically with the bottom hooks of the overload relay.

  5. Place the phase separator adaptor back on the overload relay.

  6. Push it inwards to lock it automatically with a click.

  7. Connect the overload relay downstream of the contactor using the straight bars.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.