DOCA0189EN–05

About the Book

Document Scope

Use this guide to:

  • Familiarize yourself with the mechanical and electrical characteristics of the components of TeSys Giga Series :

    • TeSys Control-Giga Contactors

    • TeSys Protect-Giga Electronic Overload Relays

  • Assemble and wire the contactors and overload relays .

Validity Note

This installation guide is valid for TeSys Control-Giga Contactors
and TeSys Protect-Giga Electronic Overload Relays with configurations as mentioned below:

  • 3-pole and 4-pole contactors :

    • 10 AC-3 ratings in 3 sizes:

      • 115–150–185–225 A

      • 265–330–400–500 A

      • 630–800 A

    • 2 types of contactors :

      • TeSys Giga Contactors - Advanced version

      • TeSys Giga Contactors - Standard version

  • Overload relays: 4 current rating ranges in 3 sizes:

    • 28–115 A and 57–225 A

    • 125–500 A

    • 160–630 A

The availability of some functions described in this guide depends on physical modules installed on the contactors and overload relays .

Online Information

The information contained in this document is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.

The technical characteristics of the devices described in the present document also appear online. To access the information online, go to the Schneider Electric home page www.se.com.

The technical characteristics presented in this guide should be the same as those that appear online. If you see a difference between the information contained in this guide and online information, use the online information.

For product compliance with environmental directives such as RoHS, REACH, PEP, and EOLI, go to www.se.com/green-premium .

Related Documentation

Document title

Description

Document number

TeSys Control - Giga Contactors and TeSys Protect - Giga Electronic Overload Relays Catalogue

Describes about the contactors and overload relays

LVCATESG_EN

TeSys Control Giga Series – Contactors – Instruction Sheet

Describes how to install the contactors

GDE2324401

TeSys Protect Giga Series – Electronic Thermal Overload Relays – Instruction Sheet

Describes how to install the overload relays

NNZ5249001

TeSys Control Giga Series – Auxiliary Contacts with Push-in Terminals – Instruction Sheet

Describes how to install the auxiliary contacts with push-in terminals

NNZ5266201

TeSys Control Giga Series – Retrofit Kit for Contactors – Instruction Sheet

Describes how to mount the contactors on plate using the retrofit kit

NNZ4443401

TeSys Control Giga Series – Remote Wear Diagnostic Module – Instruction Sheet

Describes how to mount the remote wear diagnostic module

NNZ4807901

TeSys Control Giga Series – Power Connection Accessories – Instruction Sheet

Describes how to mount the power connection accessories

NNZ4793901

Tesys Control Giga Series - Flexible Terminal Extensions - Instruction Sheet

Describes how to connect a moulded case circuit breaker to a LC1G contactor

NNZ9700101

TeSys Control Giga Series – Cable Memory – Instruction Sheet

Describes how to mount the cable memory

NNZ5141101

TeSys Control Giga Series – Control Module – Instruction Sheet

Describes how to mount the control module

NNZ5142501

TeSys Control Giga Series – Switching Module – Instruction Sheet

Describes how to mount the switching module

NNZ5266601

TeSys Control Giga Series – IP20 Terminal Shrouds for LC1G115-500 Contactors – Instruction Sheet

Describes how to mount IP20 terminal shrouds on LC1G115-500 contactors

NNZ4804701

Tesys Control Giga Series - IP20 Terminal Shrouds for LC1G630-800 Contactors - Instruction Sheet

Describes how to mount IP20 terminal shrouds on LC1G630-800 contactors

JYT9976501

TeSys Control Giga Series – Combination Accessories – Instruction Sheet

Describes how to mount the mechanical interlock and coupling bars

NNZ4813501

TeSys Control Giga Series – Phase Separator – Instruction Sheet

Describes how to mount the phase separator

JYT2250601

TeSys Control Giga Series – Push-in Terminal Adapter – Instruction Sheet

Describes how to mount the push-in terminal adapter

NNZ5142001

TeSys Protect Giga Series – Mounting Base – Instruction Sheet

Describes how to mount the stand alone overload relay on the mounting base

NNZ4806801

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.