DOCA0189EN–05

Weights

This section describes the weights for the TeSys Control-Giga contactors and TeSys Protect-Giga electronic overload relays .

Device

Number of poles

Commercial references

Weight

Advanced contactor

3P

LC1G115–225

5.4 kg (11.9 lb)

LC1G265–500

8.5 kg (18.74 lb)

LC1G630–800

17.3 kg (38.14 lb)

4P

LC1G1154–2254

6.1 kg (13.44 lb)

LC1G2654–5004

10.7 kg (23.58 lb)

LC1G630–800

22 kg (48.50 lb)

Standard contactor

3P

LC1G115–225

4.6 kg (10.14 lb)

LC1G265–500

8.2 kg (18.07 lb)

LC1G630–800

14.2 kg (31.3 lb)

4P

LC1G1154–2254

5.2 kg (11.46 lb)

LC1G2654–5004

8.7 kg (19.18 lb)

LC1G630–800

18 kg (39.68 lb)

Overload relay

3P

LR9G115-225

0.80 kg (1.75 lb)

LR9G500

1.33 kg (2.92 lb)

LR9G630

2.23 kg (4.91 lb)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.