DOCA0189EN–05

Control Module Replacement

  1. Take out the new control module from the box for replacement.
  2. Insert the control module on the contactor.
  3. Push on the screws fixing the control module on the contactor with a screwdriver.
  4. Turn the screws 90° clockwise to lock the control module.
  5. Put the flip cover back on the control module.
  6. Put back the control terminal blocks.
  7. Tighten the control terminal blocks at the right torque.
  8. Put back the auxiliary contact modules.
  9. On advanced control module, set the PLC Input switch in the same position as on the removed control module.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.