DOCA0189EN–05

Switching Module Replacement

  1. Open the flip cover under the control module.
  2. Release the switching modules screws (one screw per switching module) using an Allen key.
  3. Push up the switching module to unlock and remove it.
    NOTE: Clean the accessible parts of the contactor and visually check the overall condition of the contactor.
  4. Recycle the switching modules.
  5. Take out the new switching modules from the box for replacement.
  6. Push down the switching modules to lock it on the contactor.
  7. Tighten the switching modules screws (one screw per switching module) at the right torque.
  8. Put the flip cover back on the control module.
  9. Reset the wear diagnosis indication.

Contactor

Tool

Length of Allen Key (L)

Torque

Screws

LC1G115-225

Allen key

≥ 95 mm (≥ 3.74 in.)

0.8 ± 0.08 N•m (7 ± 0.7 lb-in)

M4

LC1G265-500

Allen key

≥ 115 mm (≥ 4.52 in.)

1 ± 0.1 N•m (8.8 ± 0.88 lb-in)

M4

LC1G630-800

Allen key

≥ 115 mm (≥ 4.52 in.)

3 ± 0.3 N•m (26.5 ± 2.65 lb-in)

M6

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.