DOCA0189EN–05

With Remote Wear Diagnosis Module

On advanced contactors with optional remote wear diagnosis module, the wear diagnosis indication must be reset on remote wear diagnosis module.

After wear detection, the Reset button on the remote wear diagnosis module is on the right.

To reset the wear diagnosis indication after replacement of the switching modules, switch the Reset button to the left.

After reset and after power on A1-A2, the contactor is in reset sequence for 10 s: the diagnosis LED is blinking, and the contactor remains open. It closes after the 10 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.