DOCA0189EN–05

Installation of the Star-Delta Connection Kits

This section describes the installation procedure of star-delta connection kits on the power terminals of the contactors. Refer to step 9 and 10 for the installation of the star bar connection kit only.

  1. Place the line-delta coupling bar beside the upstream power terminals of the line and delta contactors.

  2. Place the bars to connect the line on the upstream power terminals of the line contactor.

  3. Insert the screws and washers through the coupling bars and power terminals. Tighten the screws at the right torque.

  4. Place the bars to connect the motor on the downstream power terminals of the line contactor.

  5. Insert the screws and washers through the coupling bars and power terminals. Tighten the screws at the right torque.

  6. Place the star-delta coupling bar beside the downstream power terminals of the star and delta contactors.

  7. Place the bars to connect the motor on the downstream power terminals of the delta contactor.

  8. Insert the screws and washers through the coupling bars and power terminals. Tighten the screws at the right torque.

  9. Place the star coupling bar beside the upstream power terminals of the star contactor.

  10. Insert the screws and washers through the coupling bars and power terminals. Tighten the screws at the right torque.

Contactor

Tool

Torque

Screws

LC1G115-225

Allen key

18 ± 1.8 N•m (159 ± 15.9 lb-in)

M8

LC1G265-500

Inner hexagon

35 ± 3.5 N•m (310 ± 31 lb-in)

M10

LC1G630-800

Inner hexagon

58 ± 5.8 N•m (513 ± 51.3 lb-in)

M12

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.